PKCS-HSE demo run fail on RDB3 with QSPI image based on SDK BSP35 release

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PKCS-HSE demo run fail on RDB3 with QSPI image based on SDK BSP35 release

Jump to solution
1,392 Views
hittzt
Senior Contributor I

Hi,

 

I just test pkcs-hse demo on RDB3 board with QSPI flash boot, and the board uses a EMMC partition as rootfs(which is programed into EMMC device in previous), but the demo failed with following error:

root@nxp-s32g:~# hse-secboot -f -d /dev/mmcblk0
[INFO] Formatting HSE key catalog
hse: failed to open uio0
[ERROR] Failed to open HSE device - error 2
root@nxp-s32g:~# dmesg | grep uio
[ 2.199250] hse-uio 40210000.mu0b: firmware not found

 

The /dev/mmcblk0 is the EMMC device, and the HSE firmware has been preloaded with a full atf image into EMMC device.

The whole boot log is attached.

 

Would please help check the issue?

 

Thanks,

Zhantao

Tags (1)
0 Kudos
Reply
1 Solution
1,361 Views
hittzt
Senior Contributor I

Hi,

 

I have resolved the issues stated previously.

So I will close this ticket.

 

Thanks for your help anyway.

 

Regards,

Zhantao

View solution in original post

0 Kudos
Reply
2 Replies
1,381 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

At this moment, HSE related information is confidential and cannot be shared under a public channel. Also, RDB3 platform is based under S32G3 platform which at this moment is under control of distribution.

Please, help us opening a ticket on our NXP online service or sending this inquiry to your local NXP representative, for them to channel it through the correct medium.

We do apologize for the inconvenience this may cause, have a great day.

0 Kudos
Reply
1,362 Views
hittzt
Senior Contributor I

Hi,

 

I have resolved the issues stated previously.

So I will close this ticket.

 

Thanks for your help anyway.

 

Regards,

Zhantao

0 Kudos
Reply