PFE2 not working with correct pinux in sgmii mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PFE2 not working with correct pinux in sgmii mode

300件の閲覧回数
khan_misbah
Contributor III

Dear All,

I am using a custom s32g2 based hardware platform in which PFE2 is designed to work as "sgmii" using Serdes0 XPCS_1 channel 0

There is a PHY "TJA1104B" used in design 

The pin details of MDC/MDIO is as mentioned in the the Schematic section attached.

The dts settings are:

---------------------

&pfe_mdio2 {
                  status = "okay";

                  /* TJA1104B */
                  pfe_mdio_b_phy2: ethernet-phy@2 {
                            reg = <0x3>;
                    };

}; 

&pfe_netif2 {
             status = "okay";
            phy-mode = "sgmii";
            phy-handle = <&pfe_mdio_b_phy2>;
             managed = "in-band-status";
};

pfe2mdioa_pins: pfe2mdioa_pins {
    pfe2mdioa_grp0 {
        pinmux = <S32CC_PINMUX(82, FUNC2)>;
       //pinmux = <S32CC_PINMUX(80, FUNC1)>;
       output-enable;
       slew-rate = <S32CC_FAST_SLEW_166MHZ>;
};

pfe2mdioa_grp1 {
         pinmux = <S32CC_PINMUX(79, FUNC2)>;
        //pinmux = <S32CC_PINMUX(81, FUNC2)>;
         output-enable;
        input-enable;
        slew-rate = <S32CC_FAST_SLEW_166MHZ>;
};

pfe2mdioa_grp2 {
        pinmux = <S32CC_PINMUX(877, FUNC3)>;
       //pinmux = <S32CC_PINMUX(877, FUNC2)>;
       };
};image (1).pngimage (2).pngimage (3).png

image.png

***********************************************************************
The problem is correct mux setting which is commented above does not work (Pin 80,81), but the which is UN-commented as above works (Pin 82,79)

This is very strange.
Can you suggest as how this is possible ? 

 
Regards,
Misbah
タグ(3)
0 件の賞賛
返信
3 返答(返信)

252件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @khan_misbah 

Thanks for your reply, and glad to hear that the issue has been solved.

I have checked the link you shared, the topic is handled by my colleague, he will continue the support.

 

BR

Chenyin

0 件の賞賛
返信

272件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @khan_misbah 

Thanks for your post.

1. Per your description, if connecting the PHY to the S32G2 like the following:

chenyin_h_0-1757562505435.png

Then setting the corresponding dts(79, 82), the PFE2 could work correctly, is it right?

2. If reworking the board, connect the PHY to S32G2 like the following:(no any other modification on the schematic?)

chenyin_h_2-1757562714642.png

With only corresponding dts settings modification(80, 81), the PFE2 could not work as expected?

3. Would you mind also sharing the part number of the S32G2 used?

Thanks 

 

BR

Chenyin

 

 

 

 

0 件の賞賛
返信

258件の閲覧回数
khan_misbah
Contributor III

I Chenyin,

I have made it work, the issue was PHY address. When i changed it to correct value with correct pin mux (80,81) its working in the kernel.

Now i have another issue that the same device tree setting is not working in uboot. Detail in below ticket:

https://community.nxp.com/t5/S32G/PFE2-in-sgmii-mode-working-in-kernel-but-not-in-u-boot/m-p/2167244...

Regards,
Misbah
0 件の賞賛
返信