PFE power consumption

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PFE power consumption

4,015件の閲覧回数
Daniel_Wax
NXP Employee
NXP Employee

Im trying to help a customer determine the power consumption if only one M7 pair and the PFE are enabled.  All A53s are shut down and the other two M7s are shut down.  All other peripherals not being used.  Is there are Power consumption info on the PFE?

0 件の賞賛
返信
4 返答(返信)

3,979件の閲覧回数
Bulat
NXP Employee
NXP Employee

Please take a look at the applications notes AN13299 (S32G2 Power Estimations) and AN12952 (S32Gx Power Saving Techniques), these relates to power consumptions. In particular the first one provides dynamic power numbers for the cores and PFE modules.

 

0 件の賞賛
返信

3,961件の閲覧回数
Daniel_Wax
NXP Employee
NXP Employee

Thanks.  I now see a 320mW for PFE in AN13299.  AN12952 does not exist anywhere I can see.  Not on the public site and not in DOCSTORE

0 件の賞賛
返信

3,954件の閲覧回数
Bulat
NXP Employee
NXP Employee

It is strange... The AN12952 can be found among other app notes on the S32G2 home page:

https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/s32g-vehicle-network-pro...

 

Here is a direct link:

https://www.nxp.com/webapp/Download?colCode=AN12952

 

0 件の賞賛
返信

3,912件の閲覧回数
Daniel_Wax
NXP Employee
NXP Employee

@Bulat do you think this looks correct for maximum power consumption looks around 6W(max core:4.5W + IOs: ~1.5W) and it might need cooling system for processor.  Do any customers think that cooling might be needed?  Is the guess at S32G3 in the ballpark?

 

 

 

power (mW)

remark

S32G274

4500

 

Others

1500

 

4  additional A53

260

130 * 2 dynamic power

one additional M7

30

dynamic power

core clock 1.3G

6664

1.3 * ( 4500 + 260)

 

 

 

S32G399

8194

6664 + 1500 + 30

 

0 件の賞賛
返信