Open GoldVIP S32G399 M7 bootloader EB project

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Open GoldVIP S32G399 M7 bootloader EB project

2,740件の閲覧回数
AntZeng
Contributor I

How to open the Bootloader project?Do I need to pay for EB lisence? I have installed GoldVIP EB Temporary lisence ,and I can compile the APP project。

 

Version:GoldVIP1.11.0

project:realtime\s32g399ardb3\bootloader\workspace\Bootloader_S32G3XX_ASR_4.4_M7(failed)

project:realtime\s32g399ardb3\can-gw\workspace\goldvip-gateway(Ok)

ラベル(1)
タグ(1)
0 件の賞賛
返信
5 返答(返信)

2,629件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @AntZeng

Thanks for the update.

According to the GoldVIP UM, the Elektrobit ACP for S32G3 8.8.7 is required, I suggest installing it for a trial, to check if there are still license issues. The tool could be downloaded from your account list, like the following:

 

chenyin_h_0-1712821635862.pngchenyin_h_0-1712821635862.png

 

 

Best Regards

Chenyin

0 件の賞賛
返信

2,659件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @AntZeng

Thanks for the feedback.

Would you please help to provide the version of EB? A snapshot after clicking help->EB tresos details is preferred.

For the 3 modules listed in your first picture, they are part of the Safety packages, which is the premium software, for which we recommend contacting your local NXP FAE/DFAE/representative for more information on this regard.

 

Best Regards

Chenyin

0 件の賞賛
返信

2,646件の閲覧回数
AntZeng
Contributor I

AntZeng_0-1712802193248.jpegAntZeng_0-1712802193248.jpeg

the version of EB,28.2.

0 件の賞賛
返信

2,687件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @AntZeng

Thanks for the question

May I know what is the actually error you met during the building for Bootloader_S32G3XX_ASR_4.4_M7 project? Any logs/snapshots related with the errors?

 

Best Regards

Chenyin

0 件の賞賛
返信

2,677件の閲覧回数
AntZeng
Contributor I

1.Three modules are not installed。and I can't find  these modules。

krwPYzyUkL.jpgkrwPYzyUkL.jpg

2.remove Not installed modules,  generate project ,Error :"all modoules  no lisence"。 

4c6TtQ6xMH.jpg4c6TtQ6xMH.jpg

3、but I can open APP project(\GoldVIP-S32G3-1.11.0\realtime\s32g399ardb3\can-gw\workspace\goldvip-gateway)。lisence file。(GoldVIP Temporary lisence,3 months)

AntZeng_0-1712642295640.jpegAntZeng_0-1712642295640.jpeg

 

 

0 件の賞賛
返信