Lauterbach support on Goldbox

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Lauterbach support on Goldbox

ソリューションへジャンプ
2,028件の閲覧回数
Balakrishna971
Contributor II

Hi, 

I see there are two JTAG ports on NXP Goldbox, please confirm if Goldbox is compitable with Lauterbach to debug both A53 and M7 cores? Please share the useful links.

 

Thanks,

Bala

0 件の賞賛
返信
1 解決策
2,013件の閲覧回数
steffen_krausse
Contributor III

Hello Bala,

There are actually three related connectors for the debugger. I guess you intension is to debug the S32G controller only and not the additional SJA1110 controller on the board. In this case you can ignore J44 (10 pin connector) and use for debugging J48 (20 pin connector) with a standard Arm IDC20A debug cable. With the debugger connected to this port you can use the scripts being part of your TRACE32 installation:

CD.DO ~~/demo/arm/hardware/s32g2/s32g-vnp-evb/*

and select the right debug use case for your selve. If you want to use additionally an external trace tool, an HSSTP preprocessor or a Power trace Serial can be additionally connected to J57 (40 pin AURORA header).

Best Regards,
Steffen.

元の投稿で解決策を見る

1 返信
2,014件の閲覧回数
steffen_krausse
Contributor III

Hello Bala,

There are actually three related connectors for the debugger. I guess you intension is to debug the S32G controller only and not the additional SJA1110 controller on the board. In this case you can ignore J44 (10 pin connector) and use for debugging J48 (20 pin connector) with a standard Arm IDC20A debug cable. With the debugger connected to this port you can use the scripts being part of your TRACE32 installation:

CD.DO ~~/demo/arm/hardware/s32g2/s32g-vnp-evb/*

and select the right debug use case for your selve. If you want to use additionally an external trace tool, an HSSTP preprocessor or a Power trace Serial can be additionally connected to J57 (40 pin AURORA header).

Best Regards,
Steffen.