Lauterbach script

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Lauterbach script

1,709 Views
Abhiram_m_s
Contributor I

Hello , i tried to attach a lauterbach script for s32g3 rdb3. I have been getting an error saying "Target processor in reset". Can you please let me know what the error is and also which script to install.

Thank you.

0 Kudos
Reply
1 Reply

1,693 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @Abhiram_m_s

Thanks for the question.

  1. Regarding to the "Target processor in reset", the following link would be the official reference: https://support.lauterbach.com/kb/articles/arm-system-up-system-mode-attach-returns-target-reset-det...

You may try to disconnect the debug cable and reconnect with the board powered off, then power on the board and check if the problem persists.

  1. Regarding to the script, it depends on which package/examples you are using, in general,  in the RTD SW package, there would be cmm file existed for debugging.

For example, if you are working with the Integration Reference Examples, the following scripts could be used for reference: Integration_Reference_Examples_S32G3_2023_02\code\framework\realtime\swc\bootloader\platforms\S32G3XX\build\cmm

Hope it helps.

 

Best Regards

Chenyin

0 Kudos
Reply