LLEC getting started guide& firmware userguide

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LLEC getting started guide& firmware userguide

Jump to solution
4,002 Views
brian_w
Contributor III

Hi,

Where can I find the LLEC getting started guide and LLCE firmware userguide?

Thanks a lot!

0 Kudos
Reply
1 Solution
3,986 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

The User Guide is provided once the LLCE package is installed. It should be located on the following address:

"C:/nxp/S32G_LLCE_1_0_4/firmware/llce_interface/doc/LLCE_firmware_user_guide.pdf"

It may vary depending on where you installed it, but it is given after the installation. The Reference Manual also provides information regarding LLCE [Chapter 54, Page 2450, S32G2 Reference Manual, Rev. 6, 11/2022].

Please, let us know if this information was helpful or not.

View solution in original post

0 Kudos
Reply
4 Replies
3,987 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

The User Guide is provided once the LLCE package is installed. It should be located on the following address:

"C:/nxp/S32G_LLCE_1_0_4/firmware/llce_interface/doc/LLCE_firmware_user_guide.pdf"

It may vary depending on where you installed it, but it is given after the installation. The Reference Manual also provides information regarding LLCE [Chapter 54, Page 2450, S32G2 Reference Manual, Rev. 6, 11/2022].

Please, let us know if this information was helpful or not.

0 Kudos
Reply
3,755 Views
Pashan
Contributor II

Hello Daniel-Aguirre,

After I install the software, I see the following folder as empty 

C:\NXP\S32G_LLCE_1_0_5\firmware\llce_interface\doc

Can you please confirm whether the LLCE_firmware_user_guide.pdf file is present in the 1.0.5 Release Bundle?

Best regards

 

0 Kudos
Reply
3,746 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

We are seeing the file available under the provided path:

DanielAguirre_0-1692728613983.pngDanielAguirre_0-1692728613983.png

Could be that it was not installed correctly.

Please, let us know.

0 Kudos
Reply
3,744 Views
Pashan
Contributor II
Hello Daniel,
Thank you.
I reinstalled and I can find the file.
Best regards