LLCE routing process flow

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LLCE routing process flow

Jump to solution
2,167 Views
kazuki
Contributor II

Please tell me about the flow of LLCE routing processing.

If LLCE's CAN2CAN routing is configured, unrouted CAN calls an interrupt handler and is processed.

I believe that CAN for which LLCE does not have routing settings is not processed by the interrupt handler.

Are there any materials or explanations that can answer this question?

0 Kudos
Reply
1 Solution
2,148 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

We might be misunderstanding your question. If so, we apologize.

We see the following diagram is provided on regards of LLCE internal routing:

DanielAguirre_1-1709301249003.png

We can also recommend looking into the following LLCE training, in which the above diagram is provided as well as more information on regards of the LLCE subsystem:

Understanding the S32G2 LLCE | NXP Semiconductors

Please, let us know.

View solution in original post

2 Replies
2,149 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

We might be misunderstanding your question. If so, we apologize.

We see the following diagram is provided on regards of LLCE internal routing:

DanielAguirre_1-1709301249003.png

We can also recommend looking into the following LLCE training, in which the above diagram is provided as well as more information on regards of the LLCE subsystem:

Understanding the S32G2 LLCE | NXP Semiconductors

Please, let us know.

2,112 Views
kazuki
Contributor II

hello

I wanted to see the processing of LLCE, but I understood that I couldn't see it because it was provided by FW.

Thank you for answering.