LLCE LIN calculated baudrate

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LLCE LIN calculated baudrate

Jump to solution
2,408 Views
Alex_mjl
Contributor II

Hi NXP team,

    I would like to know how LLCE LIN's baudrate is calculated?  I set the baudrate to 9600 in the S32DS configuration menu.  And then it automatically generates the corresponding value, and I want to know how this value is calculated?

Alex_mjl_0-1721041294843.pngAlex_mjl_1-1721041320396.png

 

0 Kudos
Reply
1 Solution
2,391 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

LLCE LIN interfaces are LINFlexD based. The following is told under the S32G2 Reference Manual [Page 2250, S32G2 Reference Manual, Rev. 8, February 2024]:

DanielAguirre_0-1721054507984.png

Please, let us know.

View solution in original post

0 Kudos
Reply
3 Replies
2,392 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

LLCE LIN interfaces are LINFlexD based. The following is told under the S32G2 Reference Manual [Page 2250, S32G2 Reference Manual, Rev. 8, February 2024]:

DanielAguirre_0-1721054507984.png

Please, let us know.

0 Kudos
Reply
2,369 Views
Alex_mjl
Contributor II
I've found the relationship between them. Thank you
0 Kudos
Reply
2,371 Views
Alex_mjl
Contributor II

Hi Daniel,

Got it. But the initialization of LLCE LIN is done through the S32G and the shared memory between it. So if I want to set the baud rate of LLCE LIN in the initialization, I can only do it through this variable in the sharememory structure. That's why I want to know how this value is calculated.

0 Kudos
Reply