LLCE Interrupt latency

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LLCE Interrupt latency

1,140件の閲覧回数
Naveenkumar_Muthusamy
Contributor IV

Hi,

we are using all the four LLCE LINFLEXD channels as UART with LLCE interrupt forwarding in our s32g2 rev2 system.

in Linflexd, FOR UART we have enabled the RX interrupts.

Here RX interrutpts are always enabled, and as soon as data is received, ISR is exceuted and data is stored in a circular buffer.

This data is taken by application for further processing.

The issue we are seeing is that the interrupt latency for RX seems to be sometimes more, i.e ISR is called or executed with a higher latency period.

as per our previous conversations with the NXP, it was understood that the only one ISR is available for all the channles of LLCE LINFLEXD.

is there any way that we can reduce the interrupt latency, or is there any way to create ISR for each LINFLEXD channels, which would really improve our system performance.

タグ(3)
0 件の賞賛
返信
1 返信

1,123件の閲覧回数
Naveenkumar_Muthusamy
Contributor IV

hi @Daniel-Aguirre ,

any update on this issue?

 

0 件の賞賛
返信