LLCE-CAN AND LLCE-LOGGER

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LLCE-CAN AND LLCE-LOGGER

2,211件の閲覧回数
leehaonan
Contributor II

Can llce-can and llce-logger coexist, or is it possible to switch between them in U-Boot?

I have appended both features to DISTRO_FEATURES using 'DISTRO_FEATURES_append = " llce-can llce-logger "', but when I run 'ifconfig -a', I find that llce-can is still the default

0 件の賞賛
返信
3 返答(返信)

2,202件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

With which BSP version are you working with? Under BSP33.0, the following is told:

"The driver is able to operate in two modes: along with Linux LLCE CAN driver or in scenarios where the LLCE CAN host management is part of an another software stack."

Please, let us know.

0 件の賞賛
返信

2,172件の閲覧回数
leehaonan
Contributor II

My BSP Version is bsp37

0 件の賞賛
返信

2,136件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

We understand that the LLCE logger should be enabled under the "advanced/premium" LLCE-FW. Can you share the output of the following command?:

dmesg | grep llce

Under our setup, we see the following output:

DanielAguirre_0-1693862920823.png

Which is because we are using the standard LLCE-FW. 

Please, let us know.

0 件の賞賛
返信