Issue with PTP Hardware Timestamp Support in BSP 36

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issue with PTP Hardware Timestamp Support in BSP 36

Jump to solution
6,035 Views
steven-Yeh
Contributor I

Hi,
We are currently testing the Precision Time Protocol (PTP) functionality on our hardware. During our testing, we observed that the BSP 35 version supports hardware timestamping with ptp4l. However, upon upgrading to BSP 36 to align with Ubuntu 22, we found that BSP 36 does not support hardware timestamping.

Below are the details for both BSP versions:

  • BSP 35: Supports hardware timestamping with ptp4l.

 

root@s32g399ardb3:~# dmesg | grep Linux
[    0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[    0.000000] Linux version 5.10.145-rt74+g1594b25154a2 (oe-user@oe-host) (aarch64-fsl-linux-gcc (GCC) 10.2.0, GNU ld (GNU Binutils) 2.35.1) #1 SMP PREEMPT Tue Nov 29 10:33:39 UTC 2022
[    0.392455] pps_core: LinuxPPS API ver. 1 registered
root@s32g399ardb3:~# ptp4l -i pfe1 -m -H -s
ptp4l[15680.779]: selected /dev/ptp1 as PTP clock
ptp4l[15680.781]: port 1: INITIALIZING to LISTENING on INIT_COMPLETE
ptp4l[15680.781]: port 0: INITIALIZING to LISTENING on INIT_COMPLETE
ptp4l[15680.781]: port 1: link down
ptp4l[15680.781]: port 1: LISTENING to FAULTY on FAULT_DETECTED (FT_UNSPECIFIED)
ptp4l[15680.781]: selected local clock 0001be.fffe.beef22 as best master
ptp4l[15680.781]: port 1: assuming the grand master role
ptp4l[15680.781]: port 1: master state recommended in slave only mode
ptp4l[15680.781]: port 1: defaultDS.priority1 probably misconfigured​

 

  • BSP 36: Does not support hardware timestamping with ptp4l.
  • root@s32g399ardb3:~# dmesg | grep Linux
    [    0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
    [    0.000000] Linux version 5.15.85-rt55+gcae18cbfa3c1 (oe-user@oe-host) (aarch64-fsl-linux-gcc (GCC) 11.3.0, GNU ld (GNU Binutils) 2.38.20220708) #1 SMP PREEMPT Fri Feb 3 13:18:34 UTC 2023
    [    0.400444] pps_core: LinuxPPS API ver. 1 registered
    [    5.199079] usb usb1: Manufacturer: Linux 5.15.85-rt55+gcae18cbfa3c1 ehci_hcd
    root@s32g399ardb3:~#  ptp4l -i pfe1 -m -H -s
    ptp4l[2108.818]: selected /dev/ptp1 as PTP clock
    ptp4l[2108.820]: driver rejected most general HWTSTAMP filter
    ptp4l[2108.820]: ioctl SIOCSHWTSTAMP failed: Operation not supported
    ptp4l[2108.820]: port 1: INITIALIZING to FAULTY on FAULT_DETECTED (FT_UNSPECIFIED)
    ptp4l[2108.820]: port 0: INITIALIZING to LISTENING on INIT_COMPLETE

Could you please assist us in resolving this issue or provide any insights into the changes made in BSP 36 that might affect hardware timestamping support? Your guidance on how we might enable or work around this feature in BSP 36 would be greatly appreciated.

Thank you for your attention to this matter.

Tags (1)
0 Kudos
Reply
1 Solution
5,949 Views
RichardC
NXP Employee
NXP Employee

Hi,

I mean download the bsp36 source code and build the bsp36 manually instead of directly download it.

The version should be 1.3 instead of 1.2.

Regards,

Richard Chung.

View solution in original post

0 Kudos
Reply
6 Replies
4,584 Views
xiaoshumiao
Contributor IV

I encountered the same problem: I downloaded the source code:

git clone git://git.code.sf.net/p/linuxptp/code linuxptp

then make and make install, and the same problem occurred.

Later, I deleted the source code and installed it through apt:

sudo apt install linuxptp

and there was no such problem.

0 Kudos
Reply
5,971 Views
RichardC
NXP Employee
NXP Employee

Hi customer,

It looks you are using some version of pfe driver with issues.

Please follow the instruction on bsp36 user manual to download and build the bsp by yourself and test again.

You can use modinfo to check the module version of pfeng.

 

0 Kudos
Reply
5,955 Views
steven-Yeh
Contributor I

Hi Richard,
We are currently using the SW32G3 Linux BSP 36.0_CD image downloaded from the NXP website, and it is being implemented on the RDB3 machine. Below is the pfeng version information we obtained:

stevenYeh_0-1722566565715.png

stevenYeh_1-1722567618915.png

Could you please clarify if you mean that we need to change the pfeng version ourselves?

Additionally, we are encountering an issue where we used to be able to use phytool to read PHY data, but now we receive the error message: phy_read(-95). Is this also related to the pfeng version?

Thank you for your assistance.

0 Kudos
Reply
5,950 Views
RichardC
NXP Employee
NXP Employee

Hi,

I mean download the bsp36 source code and build the bsp36 manually instead of directly download it.

The version should be 1.3 instead of 1.2.

Regards,

Richard Chung.

0 Kudos
Reply
5,928 Views
steven-Yeh
Contributor I
Hi Richard ,

I have upgraded the pfeng version to 1.3, and it has resolved the issues we were experiencing.

Thank you for your assistance.
0 Kudos
Reply
6,020 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

We will review this with the related team and let you know the feedback from their side.

We apologize for any delay from our side.

Please, let us know.

0 Kudos
Reply