Impossible to build a project in S32DS on Ubuntu 20

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Impossible to build a project in S32DS on Ubuntu 20

2,699 次查看
curiousmindflow
Contributor II

Hello,

I encounter a compilation issue since days with S32DS 3.4 on Ubuntu 20 (it was the same case on ubuntu 18 as well).

The issue appears after the action "Update Code" in "Pins" view. The file named "Siul2_Port_Ip_Defines.h" is marked as deleted. Even if i unmarked it, it is deleted.

This issue does not appear on Windows 10. With the exact same dependencies version (32DS, RTD, IPCF etc....) than my installation on Ubuntu 20.

 

Build output:

10:52:55 **** Build of configuration Debug_RAM for project IPCF_Example_S32G274 ****
make -j8 all
Building file: ../src/main.c
Building file: ../src/sample.c
Invoking: Standard S32DS C Compiler
Invoking: Standard S32DS C Compiler
arm-none-eabi-gcc "@src/main.args" -MMD -MP -MF"src/main.d" -MT"src/main.o" -o "src/main.o" "../src/main.c"
Building file: ../generate/src/IntCtrl_Ip_Cfg.c
arm-none-eabi-gcc "@src/main.args" -MMD -MP -MF"src/sample.d" -MT"src/sample.o" -o "src/sample.o" "../src/sample.c"
Invoking: Standard S32DS C Compiler
Building file: ../generate/src/OsIf_Cfg.c
arm-none-eabi-gcc "@generate/src/IntCtrl_Ip_Cfg.args" -MMD -MP -MF"generate/src/IntCtrl_Ip_Cfg.d" -MT"generate/src/IntCtrl_Ip_Cfg.o" -o "generate/src/IntCtrl_Ip_Cfg.o" "../generate/src/IntCtrl_Ip_Cfg.c"
Invoking: Standard S32DS C Compiler
arm-none-eabi-gcc "@generate/src/IntCtrl_Ip_Cfg.args" -MMD -MP -MF"generate/src/OsIf_Cfg.d" -MT"generate/src/OsIf_Cfg.o" -o "generate/src/OsIf_Cfg.o" "../generate/src/OsIf_Cfg.c"
Building file: ../board/Clock_Ip_Cfg.c
Building file: ../board/Clock_Ip_PBcfg.c
Invoking: Standard S32DS C Compiler
arm-none-eabi-gcc "@board/Clock_Ip_Cfg.args" -MMD -MP -MF"board/Clock_Ip_Cfg.d" -MT"board/Clock_Ip_Cfg.o" -o "board/Clock_Ip_Cfg.o" "../board/Clock_Ip_Cfg.c"
Building file: ../board/Siul2_Port_Ip_Cfg.c
Invoking: Standard S32DS C Compiler
arm-none-eabi-gcc "@board/Clock_Ip_Cfg.args" -MMD -MP -MF"board/Clock_Ip_PBcfg.d" -MT"board/Clock_Ip_PBcfg.o" -o "board/Clock_Ip_PBcfg.o" "../board/Clock_Ip_PBcfg.c"
Invoking: Standard S32DS C Compiler
arm-none-eabi-gcc "@board/Clock_Ip_Cfg.args" -MMD -MP -MF"board/Siul2_Port_Ip_Cfg.d" -MT"board/Siul2_Port_Ip_Cfg.o" -o "board/Siul2_Port_Ip_Cfg.o" "../board/Siul2_Port_Ip_Cfg.c"
Building file: ../board/dcd_config.c
Finished building: ../generate/src/OsIf_Cfg.c
Invoking: Standard S32DS C Compiler
arm-none-eabi-gcc "@board/Clock_Ip_Cfg.args" -MMD -MP -MF"board/dcd_config.d" -MT"board/dcd_config.o" -o "board/dcd_config.o" "../board/dcd_config.c"

Building file: ../board/ivt_config.c
Invoking: Standard S32DS C Compiler
arm-none-eabi-gcc "@board/Clock_Ip_Cfg.args" -MMD -MP -MF"board/ivt_config.d" -MT"board/ivt_config.o" -o "board/ivt_config.o" "../board/ivt_config.c"
In file included from ../board/Siul2_Port_Ip_Cfg.h:5,
from ../board/Siul2_Port_Ip_Cfg.c:14:
../RTD/include/Siul2_Port_Ip_Types.h:46:10: fatal error: Siul2_Port_Ip_Defines.h: No such file or directory
Finished building: ../board/dcd_config.c
46 | #include "Siul2_Port_Ip_Defines.h"
| ^~~~~~~~~~~~~~~~~~~~~~~~~
compilation terminated.
make: *** [board/subdir.mk:35: board/Siul2_Port_Ip_Cfg.o] Error 1
make: *** Waiting for unfinished jobs....
../src/sample.c: In function ‘xSemaphoreTake’:
../src/sample.c:41:65: warning: unused parameter ‘timeout’ [-Wunused-parameter]
41 | static uint8_t xSemaphoreTake(SemaphoreHandle_t psema, uint32_t timeout) {
Finished building: ../src/main.c

| ~~~~~~~~~^~~~~~~

../src/sample.c: In function ‘vTaskDelay’:
../src/sample.c:50:2: warning: ‘static’ is not at beginning of declaration [-Wold-style-declaration]
Finished building: ../generate/src/IntCtrl_Ip_Cfg.c
50 | volatile static uint32 delayTimer = 0;

| ^~~~~~~~
../src/sample.c: In function ‘ctrl_chan_rx_cb’:
../src/sample.c:152:14: warning: pointer of type ‘void *’ used in arithmetic [-Wpointer-arith]
152 | strtol(mem + strlen("SENDING MESSAGES: "), &endptr, 10);
| ^
../src/sample.c:139:47: warning: unused parameter ‘instance’ [-Wunused-parameter]
139 | void ctrl_chan_rx_cb(void *arg, const uint8_t instance, int chan_id, void *mem)
| ~~~~~~~~~~~~~~^~~~~~~~
Finished building: ../board/ivt_config.c

Finished building: ../src/sample.c

Finished building: ../board/Clock_Ip_Cfg.c

Finished building: ../board/Clock_Ip_PBcfg.c

"make -j8 all" terminated with exit code 2. Build might be incomplete.

10:52:56 Build Failed. 3 errors, 4 warnings. (took 431ms)

标记 (3)
0 项奖励
回复
2 回复数

2,601 次查看
curiousmindflow
Contributor II

Hello,

As i said, i tried on Ubuntu 18 as well and it ends up with exactly the same issue.

I checked dependencies:
- S32DS -> S32DS.3.4_b201217_linux.x86_64
- S32G2 SDK -> SW32G2_S32DS_3.4.1_D2104
- RTD -> SW32G2_RTD_4.4_2.0.0_HF02_DS_updatesite_D2106
- IPCF -> SW32G2_IPCF_4.3.0_D2109_updatesite

I think they are all compatible, as with the same version, it works fine on windows 10, as i said, also.

0 项奖励
回复

2,639 次查看
bpe
NXP Employee
NXP Employee

Ubuntu 20 is not in the list of supported host operating systems of S32DS 3.4.
As of the rest, the information you provided does not allow to identify the root
cause of the problem. The symptoms you describes do not match any known problem
with S32DS. What you can do is:

  1. Make sure you are working with the most recent version of S32DS for your
    target S32 processor. For S32G2 it is 3.4.1.
  2. Make sure the rest of the software your project depends on is version-compatible.
    Check the release Notes of each package for compatibility information.
  3. It sometimes happens that packages removed for some reason and then and
    re-installed work incorrectly. Check the installation guides and release
    notes of each package for the proper installation sequence. You may need
    to re-install everything anew.
  4. If the problem persists:
    1. Register yourself with your corporate e-Mail address on NXP Website.
    2. Open a Support Case and provide a minimum steps scenario to make the
      problem visible.

 

Best Regards,
Platon

 

0 项奖励
回复