Implementation IEEE 802.1AS (version 2020) using gPTP at S32G

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Implementation IEEE 802.1AS (version 2020) using gPTP at S32G

2,634 次查看
janssen135
Contributor I

Hi,

 

I am looking the NXP documentation for the implementation IEEE 802.1AS (version 2020) using gPTP at S32G.

Can someone tell me where is the documentation?

I am wondering how to implement this topic:

1. using current AUTOSAR version, because the current AUTOSAR version only supports IEEE 802.1AS (version 2011)

2. using non AUTOSAR solution.

 

Thank you

0 项奖励
回复
1 回复

2,579 次查看
MayanksPatel
NXP Employee
NXP Employee

Hi @janssen135,

Hope you are doing well.

For the implementation of IEEE 802.1AS, there were no separate applications available but you can refer GMAC loopback example and GMAC reference manual for the same.

For enabling the 802.1AS, you need to enable the PTP Timestamp offload feature using the "MAC_PTO_Control" register and then after set the 28th bit of the "MAC_Timestamp_Control" register.

Hope this helps.

 

Regards,

Mayank s Patel

 

0 项奖励
回复