Implement ethernet function in M core for S32G399A

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Implement ethernet function in M core for S32G399A

581 次查看
xlfd_1981
Contributor III

hi NXP Experts,

I want to implement Ethernet functionality on the M core, while also ensuring that the Ethernet functionality on the A core remains normal. How can I do this? Is there any relevant code or implementation plan available?

Thanks

0 项奖励
回复
5 回复数

502 次查看
chenyin_h
NXP Employee
NXP Employee

Hello, @xlfd_1981 

You are welcome, I'd like to help.

Feel free to raise any new ticket if you have further specific questions, we would track and support it.

 

BR

Chenyin 

0 项奖励
回复

524 次查看
chenyin_h
NXP Employee
NXP Employee

Hello, @xlfd_1981 

Sure, the Ethernet communication could be implemented on M core side, I suggest reading the examples shown in PFE-MCAL for your reference.

 

BR

Chenyin

0 项奖励
回复

518 次查看
xlfd_1981
Contributor III
You're welcome! I am going to read the PFE-MCAL example. If I have any questions, I will come to you for advice. Thank you, Chenyin.
0 项奖励
回复

558 次查看
chenyin_h
NXP Employee
NXP Employee

Hello, @xlfd_1981 

Thanks for your post.

From the description you shared, I suggest referencing the PFE master/slave mode, which may fulfill your requirement, you may refer to the BSP UM and the document/examples in PFE_MCAL for details.

 

BR

Chenyin

0 项奖励
回复

548 次查看
xlfd_1981
Contributor III
Is it feasible to implement Ethernet communication on an M-core processor, have you realized this function before.
0 项奖励
回复