Implement ethernet function in M core for S32G399A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Implement ethernet function in M core for S32G399A

1,431 Views
xlfd_1981
Contributor III

hi NXP Experts,

I want to implement Ethernet functionality on the M core, while also ensuring that the Ethernet functionality on the A core remains normal. How can I do this? Is there any relevant code or implementation plan available?

Thanks

0 Kudos
Reply
5 Replies

1,352 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @xlfd_1981 

You are welcome, I'd like to help.

Feel free to raise any new ticket if you have further specific questions, we would track and support it.

 

BR

Chenyin 

0 Kudos
Reply

1,374 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @xlfd_1981 

Sure, the Ethernet communication could be implemented on M core side, I suggest reading the examples shown in PFE-MCAL for your reference.

 

BR

Chenyin

0 Kudos
Reply

1,368 Views
xlfd_1981
Contributor III
You're welcome! I am going to read the PFE-MCAL example. If I have any questions, I will come to you for advice. Thank you, Chenyin.
0 Kudos
Reply

1,408 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @xlfd_1981 

Thanks for your post.

From the description you shared, I suggest referencing the PFE master/slave mode, which may fulfill your requirement, you may refer to the BSP UM and the document/examples in PFE_MCAL for details.

 

BR

Chenyin

0 Kudos
Reply

1,398 Views
xlfd_1981
Contributor III
Is it feasible to implement Ethernet communication on an M-core processor, have you realized this function before.
0 Kudos
Reply