IPCF with FreeRTOS throwing error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IPCF with FreeRTOS throwing error

Jump to solution
3,786 Views
honeybee1881
Contributor II

I am using 

I am trying out example of IPCF with baremetal and FreeRTOS. 

Baremetal is working and I can see the output.

But when I ran IPCF example with FreeRTOS facing the below error.

 ./ipc-shm-sample_cdev.elf
ipc-shm-usr-lib: ipc_os_init(): Created Rx softirq thread with priority=99
ipc-shm-usr-lib: ipc_os_init(): done
ipc-shm-usr-lib: ipc_shm_init_instance(): initializing channels...
ipc-shm-usr-lib: ipc_shm_init_channels(): ipc shm channel 0 initialized
ipc-shm-usr-lib: ipc_buf_pool_init(): ipc shm pool 0 of chan 1 initialized
ipc-shm-usr-lib: ipc_buf_pool_init(): ipc shm pool 1 of chan 1 initialized
ipc-shm-usr-lib: ipc_buf_pool_init(): ipc shm pool 2 of chan 1 initialized
ipc-shm-usr-lib: ipc_shm_init_channels(): ipc shm channel 1 initialized
ipc-shm-usr-lib: ipc_buf_pool_init(): ipc shm pool 0 of chan 2 initialized
ipc-shm-usr-lib: ipc_buf_pool_init(): ipc shm pool 1 of chan 2 initialized
ipc-shm-usr-lib: ipc_buf_pool_init(): ipc shm pool 2 of chan 2 initialized
ipc-shm-usr-lib: ipc_shm_init_channels(): ipc shm channel 2 initialized
ipc-shm-usr-lib: ipc_shm_init_instance(): ipc shm initialized

Input number of messages to send: 10
ipc-shm-us-app: ch 0 >> 20 bytes: SENDING MESSAGES: 10
ipc-shm-usr-lib: ipc_shm_is_remote_ready(): inside remote_global->state is 0x0
ipc-shm-usr-lib: ipc_shm_unmanaged_tx(): inside ipc_shm_is_remote_ready
ipc-shm-us-app: send_ctrl_msg(): tx failed on control channelipc-shm-usr-lib: ipc_shm_free(): ipc shm released
ipc-shm-us-app: exit

 What can be the issue?

IPCF S32G-VNP-RDB3 S32G3 

 

0 Kudos
Reply
1 Solution
3,599 Views
honeybee1881
Contributor II

Hi,

Its working now with following combination versions

  • S32 Design Studio for S32 Platform
    Version: 3.5
    Build id: 240726 (Update 13)
  • FreeRTOS 4.0.2 D2307
  • S32 Real-Time Drivers Version 4.0.2 P04 is AUTOSAR 4.4.0
  • IPCF S32G 4.10.0.202405310722 

 

View solution in original post

0 Kudos
Reply
4 Replies
3,758 Views
Joey_z
NXP Employee
NXP Employee

hi,honeybee1881

Thank you for your information.

Do you use the example of IPCF_FreeRTOS_S32G399A_M7_0? How do you use the demo?

And do you try to use the IPCF sample from u-boot?

BR

Joey

0 Kudos
Reply
3,747 Views
honeybee1881
Contributor II

Hi Joey,

Yes, I do use the example of IPCF_FreeRTOS_S32G399A_M7_0 from the installation.

honeybee1881_0-1756886849571.png

 

How I use it

  • From "S32DS project from Example" I load the project.
  • Loaded the mex file its shows warning "The loaded configuration has been created by an older version of the tool. If saved, the old version of the tool may not be able to open again". Clicked on Ok.
  • I couldn't build out of the box, so I had to enable "Platform Interrupt Controller Configuration"
    honeybee1881_1-1756886930868.png
  • After giving "Update Code" it generates code
  • Build Project
  • Faced error "./Project_Settings/Startup_Code/system.c:72:14: fatal error: S32G399A_MC_CGM.h: No such file or directory"
  • Commented out the specific header and I am able to generate the "IPCF_FreeRTOS_S32G399A_M7_0.bin" 

I load the IPCF sample from the U-Boot console.

Please let me know for further queries.

0 Kudos
Reply
3,692 Views
Joey_z
NXP Employee
NXP Employee

hi,honeybee1881

Thank you for your reply.

About the issues: 

  • Faced error "./Project_Settings/Startup_Code/system.c:72:14: fatal error: S32G399A_MC_CGM.h: No such file or directory"

If you use the IPCF of version IPCF_S32G_4.10.0, please refer to the Release notes, and check the version of related package.

You need version of RTD and S32DS IDE as the attachment.

Hope this can help you.

BR

Joey

0 Kudos
Reply
3,600 Views
honeybee1881
Contributor II

Hi,

Its working now with following combination versions

  • S32 Design Studio for S32 Platform
    Version: 3.5
    Build id: 240726 (Update 13)
  • FreeRTOS 4.0.2 D2307
  • S32 Real-Time Drivers Version 4.0.2 P04 is AUTOSAR 4.4.0
  • IPCF S32G 4.10.0.202405310722 

 

0 Kudos
Reply