IPCF log error in s32g3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IPCF log error in s32g3

1,810件の閲覧回数
Abhiram_m_s
Contributor I

Hello,

We are trying to build IPCF_FreeRTOS_S32G399A_M7_0 example in IPCF 4.9.0 using S32DS 3.5.3
We built the bin file and we copied it to the FAT partition of the SD card.
When we try to run the following logs

Abhiram_m_s_0-1709295404337.png

as per the above steps, the expected output should be like

Abhiram_m_s_1-1709295504994.png

but we are not getting anything. 
We are using S32DS 3.5.3 , IPCF 4.9.0 and RTD 4.0.2 and Linux BSP 38.0.

Please let us know how to proceed.

0 件の賞賛
返信
3 返答(返信)

1,672件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @Abhiram_m_s

Thanks for the question.

The package you mentioned is AUTOSAR OS, which is not a public release.

Sorry for your inconvenience.

 

Best Regards

Chenyin

0 件の賞賛
返信

1,751件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @Abhiram_m_s

Thanks for the reply and sorry for the delay

We have the following suggestion for your reference

  1. From the IPCF 4.9.0 release notes, the following packages are with dependencies:
  • RTD_4.4_4.0.2_D2306
  • FreeRTOS_10.4.6_4.0.2_D2306
  • NXP_RTOS_4_4_148_CODEDROP_0_4_0_D2309
  • NXP Linux BSP38.0

Seems the RTD version and BSP version are correct, how about the RTOS version used in your examples?

2. You may check the logs by dmesg | grep ipc-shm after executing the commands from your previous post.

3. The default IPCF version under BSP38.0 is IPCF v4.8.0(not IPCF4.9), so that when using the examples with the default settings, it is actually BSP38.0 (with IPCF v4.8.0) + IPCF v4.9.0, Which is causing problems. If you wish to use IPCF 4.9.0, you need to also update the BSP38.0 IPCF version to v4.9.0

Hope it helps

 

 

Best Regards

Chenyin

0 件の賞賛
返信

1,677件の閲覧回数
Abhiram_m_s
Contributor I

I am not finding the link to download NXP_RTOS_4_4_148_CODEDROP_0_4_0_D2309.  Can you please share the link to download this package ? 

0 件の賞賛
返信