I encountered the following problem while building ATF. How can I solve it

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I encountered the following problem while building ATF. How can I solve it

306件の閲覧回数
lion_6
Contributor I

Makefile:1663: *** "Platform 's32g274ardb2' requires DDR_FW_BIN_PATH. Please set DDR_FW_BIN_PATH to point to the right file"

At the same time, under arm rusted firmware/build/s32g274ardb2/release, only these are available:
bl2  bl2_w_dtb.bin  bl2_w_dtb_size bl31.bin  bl31sram.bin dtb_size fip.cfgout libc libwrapper romlib
bl2.bin bl2_w_dtb.s32 bl31 bl31sram boot_info.c  fdts  lib  libfdt load_address

There is no fig.s32 file available

lion_6_0-1750392410336.png

 

0 件の賞賛
返信
1 返信

277件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @lion_6 

Thanks for your post.

From the log, seems you are working with BSP44?

chenyin_h_0-1750406013517.png

For building this version, you may have to firstly downloading the corresponding ddr firmware from you NXP account, if not available, I suggest using BSP43 for your another trial.

 

BR

Chenyin

0 件の賞賛
返信