Hw not booting up

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Hw not booting up

1,707件の閲覧回数
athul_am
Contributor II

Hi,

 Can you please let me know if quality checks are done on the NXP boards that are Shippped.

 My company acquired a S32g-VNP-RDB3 a month ago.I just started with the sd card in the box and it is giving me error

U-Boot 2020.04+g6286902c94 (Nov 17 2021 - 08:47:30 +0000)

CPU: NXP S32G399A rev. 1.1.0
Reset cause: Power-On Reset
Model: NXP S32G3XX
Board: NXP S32G399A-RDB3
DRAM: Error 3 on ddr_init
initcall sequence 000000003410be40 failed at call 00000000340a2f18 (err=3)
### ERROR ### Please RESET the board ###

What am i supposed to do now,

Thanks,

Athul

0 件の賞賛
返信
3 返答(返信)

1,661件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @athul_am 

Thanks for your reply.

Firstly, may I know which version BSP images you had created for testing? I suggest using the newer version to have a try.

Secondly, may I know if you have the S32DS installed? I suggest referencing the following link to try the DDR tools and generate related logs, we will check it later.

https://community.nxp.com/t5/S32G/S32G3-VPN-Linux-BSP-Won-t-Boot-DDR-Error/m-p/1998154#M11789

Finally, would you please share the board version? it could be usually found on the board.

Sorry for your inconvenience

 

BR

Chenyin

0 件の賞賛
返信

1,676件の閲覧回数
athul_am
Contributor II

Hi @chenyin_h ,

I have tried with the Sd card image that came with the board and also created an image and tried it I am getting the same error. I did not make any changes to the board.

Thanks for the response 

Athul

0 件の賞賛
返信

1,689件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @athul_am 

Sorry to hear that you met such issues.

May I know if you were testing the board with default SD card from the board without any modifications?

May I know if it is possible for you to test the board with the latest pre-built BSP images?

 

BR

Chenyin

0 件の賞賛
返信