How to use SAF packages with S32G

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to use SAF packages with S32G

706 次查看
xiaomu
Contributor II

Hi , there:

 I'm Using S32G_SAF_2.0.0_EVAL packages to do an experiment, But I Don't know how to build the S32_SAF_Demo And Tresos project within the folder:
    1. When i modified the launch.bat according my local environment ,and then executed it, then a error occured " ./Tresos/S32_SAF_S32G2XX_S32G274A/output/generated/src/Bist_Cfg.c:57:10: fatal error: S32_SAF_Version.h: No such file or directory "

    2. when i use EB Tresos 27.1.0 import the eb project , most of the module has errors and can not execute  genreate ,how can I resolve the problems? 

  can anyone help me ? thanks very much !!

0 项奖励
回复
1 回复

684 次查看
chenyin_h
NXP Employee
NXP Employee

Hello, @xiaomu

For information regarding SAF, since it is a premium software, given this is a public channel we do recommend going directly to your local NXP representative/FAE, for them to channel it through the correct medium.
I do apologize for your inconvenience.
 
Best Regards
Chenyin
0 项奖励
回复