How to use PFE function of S32G-VNP-RDB3 (s32g399a) based on RTOS?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to use PFE function of S32G-VNP-RDB3 (s32g399a) based on RTOS?

ソリューションへジャンプ
968件の閲覧回数
Youngsoo_do
Contributor III

We are developing S32G-VNP-RDB3 (s32g399a) based on RTOS. I know we need to use PFE to use more than one Ethernet port, but PFE requires a separate driver to be applied, and I don't know how to do that.

To rephrase my question, it is as follows.

1. How to use PFE function in S32G-VNP-RDB3(s32g399a)?

2. is there any demo file for PFE's PTP and TIME Aware Shaper features?

 

If anyone knows how to use it, please help me.... Please help...

0 件の賞賛
返信
1 解決策
860件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Below will be some comments on regards of your questions:

Q1. Is it mandatory to use Tresos to use PFE FW?

[DA]: We understand that the PFE MCAL driver is only to be used with EB Tresos. As for the license error, did you activate EB Tresos itself?

Q2. Do you know any documentation explaining how to use PFE FW in S32 Design Studio?

[DA]: At this moment, there is no up-to-date documentation for PFE MCAL under S32DS. We do apologize.

Q3. Is PFE FW used in conjunction with PFE MCAL Driver?

[DA]: We understand that there is indeed a requirement for PFE MCAL with PFE FW, since it details under the respective release notes that uses both RTD package and PFE FW.

Please, let us know.

元の投稿で解決策を見る

4 返答(返信)
947件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

On regards of PFE usage under the M7 core (which we assume is the one being used with RTOS), there is a PFE Driver for M7 MCAL, which should be available under the Automotive Software Package Manager inside the S32G3 product page (link: S32G3 Safe and Secure Vehicle Network Processor | NXP Semiconductors). The specific version needs to be paired with an specific version of RTD, which should be also available under the Automotive Software Package Manager.

As for the specifics of being implemented with RTOS, we understand that the available examples do not use RTOS. As for the specific features, we understand that they are not implemented under the available examples. We do apologize.

Please, let us know.

935件の閲覧回数
Youngsoo_do
Contributor III

I am very grateful for your response.

I went to the site you told me about and downloaded the Dirver and Firmware for PFE, and I had additional questions in the process.

Q1. Is it mandatory to use Tresos to use PFE FW?

  Q1.1. I installed the PFE FW plugin from Tresos, but when I open it in Tresos, I get a license error like in the attached picture.

Q2. Do you know any documentation explaining how to use PFE FW in S32 Design Studio?

Q3. Is PFE FW used in conjunction with PFE MCAL Driver?

 

2.png1.png

0 件の賞賛
返信
861件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Below will be some comments on regards of your questions:

Q1. Is it mandatory to use Tresos to use PFE FW?

[DA]: We understand that the PFE MCAL driver is only to be used with EB Tresos. As for the license error, did you activate EB Tresos itself?

Q2. Do you know any documentation explaining how to use PFE FW in S32 Design Studio?

[DA]: At this moment, there is no up-to-date documentation for PFE MCAL under S32DS. We do apologize.

Q3. Is PFE FW used in conjunction with PFE MCAL Driver?

[DA]: We understand that there is indeed a requirement for PFE MCAL with PFE FW, since it details under the respective release notes that uses both RTD package and PFE FW.

Please, let us know.

811件の閲覧回数
Youngsoo_do
Contributor III

Hi ! Thank you very much for your response.

about Q1

When I got the tresos from that page (link: S32G3 Safe and Secure Vehicle Network Processor | NXP Semiconductors), I could not get any confirmation regarding the license. Instead, I downloaded version 29 from the place where you can download different versions, checked the activation code, activated it, and am using it.

About Q2 and Q3

I'm having trouble using and developing it due to the lack of documentation. I will try to check the related release notes.

 

Thank you for your help. For additional questions, I will create a new session to ask.

タグ(1)
0 件の賞賛
返信