How to make both smooth running under boot ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to make both smooth running under boot ?

2,045 次查看
fengxianeric
Contributor IV

Hi,

I could make llce run by loading 0x34000000, and individually I could make ipcf run by loading address 0x34100000, so my question is how to make both simultaneously run  under boot starm7 command?  Because llce binary file above 5M size.

Thanks

0 项奖励
回复
4 回复数

1,999 次查看
nxf92355
NXP Employee
NXP Employee

Hi Eric Li

Hope you are doing well

 

Your image size is above 5 mb, did you edit sample app , right?

 

Regards ,

Tushar

0 项奖励
回复

1,995 次查看
fengxianeric
Contributor IV
THanks
Yes I need to integrate llce code into ipcf sample.
Thanks
0 项奖励
回复

1,991 次查看
fengxianeric
Contributor IV
Also, I tried modifying linker, it seems that init_ram address + image size > reset handler address, which made startm7 failed.
How to correct this issue ?
THanks
0 项奖励
回复

1,929 次查看
nxf92355
NXP Employee
NXP Employee

Hi Eric Li

Please refer Chapter 36 System RAM Controller (SRAMC) from reference manual.you can see latency and address range for core0.

Screenshot from 2023-07-04 15-28-03.png

Regards ,

Tushar

0 项奖励
回复