How to make both smooth running under boot ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to make both smooth running under boot ?

2,036件の閲覧回数
fengxianeric
Contributor IV

Hi,

I could make llce run by loading 0x34000000, and individually I could make ipcf run by loading address 0x34100000, so my question is how to make both simultaneously run  under boot starm7 command?  Because llce binary file above 5M size.

Thanks

0 件の賞賛
返信
4 返答(返信)

1,990件の閲覧回数
nxf92355
NXP Employee
NXP Employee

Hi Eric Li

Hope you are doing well

 

Your image size is above 5 mb, did you edit sample app , right?

 

Regards ,

Tushar

0 件の賞賛
返信

1,986件の閲覧回数
fengxianeric
Contributor IV
THanks
Yes I need to integrate llce code into ipcf sample.
Thanks
0 件の賞賛
返信

1,982件の閲覧回数
fengxianeric
Contributor IV
Also, I tried modifying linker, it seems that init_ram address + image size > reset handler address, which made startm7 failed.
How to correct this issue ?
THanks
0 件の賞賛
返信

1,920件の閲覧回数
nxf92355
NXP Employee
NXP Employee

Hi Eric Li

Please refer Chapter 36 System RAM Controller (SRAMC) from reference manual.you can see latency and address range for core0.

Screenshot from 2023-07-04 15-28-03.pngScreenshot from 2023-07-04 15-28-03.png

Regards ,

Tushar

0 件の賞賛
返信