How to decrease the time(5 secs to 1 sec) to publish data to cloud from fleetwise on goldvip

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to decrease the time(5 secs to 1 sec) to publish data to cloud from fleetwise on goldvip

ソリューションへジャンプ
2,078件の閲覧回数
sonalip94
Contributor III

Hello @Daniel-Aguirre

I am trying to reduce the time to publish the data to the cloud. By default it is 5000ms and i tried to change this by changing "publishToCloudParameters": {
"maxPublishMessageCount": 1000  / 500,
"collectionSchemeManagementCheckinIntervalMs": 5000 / 1000
}, 

in /etc/aws-iot-fleetwise/goldvip-config.json file.

But, this change is not reflected in the database and i still see the data is published every 5 secs to the cloud.

Can you guide me with how this can be achieved?

887309314nxp-goldbox-innxp-goldbox-in-1681197205-campaignVehicle.OBD.EngineSpeed2023-04-11 07:25:44.7880000001600.0-
887309314nxp-goldbox-innxp-goldbox-in-1681197205-campaignVehicle.OBD.Speed2023-04-11 07:25:44.78800000060.0-
887309314nxp-goldbox-innxp-goldbox-in-1681197205-campaignVehicle.OBD.AmbientAirTemperature2023-04-11 07:25:44.78800000026.0-
887309314nxp-goldbox-innxp-goldbox-in-1681197205-campaignVehicle.OBD.ThrottlePosition2023-04-11 07:25:44.78800000065.88235294117646-
887309314nxp-goldbox-innxp-goldbox-in-1681197205-campaignVehicle.OBD.FuelLevel2023-04-11 07:25:44.78800000093.72549019607843-
887309314nxp-goldbox-innxp-goldbox-in-1681197205-campaignDTC_P01232023-04-11 07:25:49.764000000-true
889875715nxp-goldbox-innxp-goldbox-in-1681197205-campaignVehicle.OBD.EngineSpeed2023-04-11 07:25:49.8080000001700.0-
0 件の賞賛
返信
1 解決策
2,011件の閲覧回数
sonalip94
Contributor III

Yes Mayank,

I saved the json and re-started the fleetwise agent as well but that did not help.

The Solution for this is to change the below parameters as well so that the fleetwise service requests the CAN data every one second and publishes to the cloud.

 

        "pidRequestIntervalSeconds": 1,
        "dtcRequestIntervalSeconds": 1,

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,028件の閲覧回数
MayanksPatel
NXP Employee
NXP Employee

Hi @sonalip94,

Hope you are doing well.

Are you saving the .json file after making changes to it?

Also, re-configure the AWS IoT Fleetwise agent (Step mentioned in the user Manual) and deploy it again.

 

Hope this helps you.

 

Thanks,

Mayank s Patel

0 件の賞賛
返信
2,012件の閲覧回数
sonalip94
Contributor III

Yes Mayank,

I saved the json and re-started the fleetwise agent as well but that did not help.

The Solution for this is to change the below parameters as well so that the fleetwise service requests the CAN data every one second and publishes to the cloud.

 

        "pidRequestIntervalSeconds": 1,
        "dtcRequestIntervalSeconds": 1,

 

0 件の賞賛
返信