How to compile a new application layer program using bitbake for BSP35.0 of S32G274

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to compile a new application layer program using bitbake for BSP35.0 of S32G274

1,049 次查看
sdx111
Contributor II

1、How to compile a new application layer program using bitbake for BSP35.0 of S322G274?And how to add the new formula, please explain in detail.

2、Is the executable file under this path an executable file in the file system? Why do I change the FSL - auto - yocto - bsp35.0 / build_s32g274ardb2 / TMP/work/cortexa53 - crypto - FSL - Linux/can - utils / 2020.02.04 - r0 / git directory path canf After dtest.c, compile and execute bitbake fsl-image-auto-C compile. FSL - auto - yocto - bsp35.0 build_s32g274ardb2 / TMP/work/s32g274ardb2 - FSL - Linux/FSL - image - auto / 1.0 - r0 / rootfs/usr/bin directory canfdt Hasn't est changed?

sdx111_0-1746789032178.png

 

标记 (1)
0 项奖励
回复
1 回复

1,019 次查看
chenyin_h
NXP Employee
NXP Employee

Hello, @sdx111 

Thanks for your post.

May I know if you want to add 3rd party software package or your own code to build in Yocto with BSP35?

Since Yocto is a 3rd-tool, there is not formal document from NXP to explain the details of Yocto, I suggest referencing the https://docs.yoctoproject.org/ for details of Yocto itself.

 

BR

Chenyin

0 项奖励
回复