Headless mode checkbox for CAN LLCE example S32G3

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Headless mode checkbox for CAN LLCE example S32G3

885 次查看
Abhiram_m_s
Contributor I

Hello,

We are trying to build Can_Llce_DS_Can2Can_S32G399A_M7 example in LLCE 1.0.7.

We are following the description, there is a point which mentions following :

Abhiram_m_s_0-1709295132621.png

Where do we find the checkbox? 
We are using S32DS 3.5.3 , RTD 4.0.2 and LLCE 1.0.7


 

 

0 项奖励
回复
1 回复

842 次查看
chenyin_h
NXP Employee
NXP Employee

Hello, @Abhiram_m_s

Thanks for the question and sorry for the delay.

You may try reference the following:

ConfigTools->Peripherals

chenyin_h_0-1709780771048.png

Then press Can_43_LLCE_1->CanGeneral

chenyin_h_1-1709780771056.png

Stroll down to find the two options related with headless mode as decribed, press the plus icon and then the checkbox could be shown.

chenyin_h_2-1709780771063.png

Hope it helps.

 

Best Regards

Chenyin

0 项奖励
回复