GoldBox-3 physicals and electrical information

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

GoldBox-3 physicals and electrical information

跳至解决方案
426 次查看
Shrek78
Contributor I

Hello,

Is there any information on physicals and electrical interfaces for the GoldBox-3?

  • Acceleration / Vibrations / Stiffness resistance based on specific standart
  • Min Max for temperature and humidity
  • Power consumption
  • electromagnetic compatibility (EMC)
  • is it rugged
0 项奖励
回复
1 解答
407 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

We understand that this information is not provided. We do apologize.

The information that may be available is on regards of temperature, which is the following (only for RDB2):

"RDB2 is designed for room temperature environment.

The board may work abnormally or be damaged in the high/low temperature test."

And about rugged (we think so?):

DanielAguirre_0-1707922050902.png

Still, help us contacting your local NXP representative/FAE/DFAE, since they may more information available than the one we have through this channel. We do apologize.

Please, let us know.

在原帖中查看解决方案

0 项奖励
回复
1 回复
408 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

We understand that this information is not provided. We do apologize.

The information that may be available is on regards of temperature, which is the following (only for RDB2):

"RDB2 is designed for room temperature environment.

The board may work abnormally or be damaged in the high/low temperature test."

And about rugged (we think so?):

DanielAguirre_0-1707922050902.png

Still, help us contacting your local NXP representative/FAE/DFAE, since they may more information available than the one we have through this channel. We do apologize.

Please, let us know.

0 项奖励
回复