GoldBox-3 physicals and electrical information

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GoldBox-3 physicals and electrical information

Jump to solution
399 Views
Shrek78
Contributor I

Hello,

Is there any information on physicals and electrical interfaces for the GoldBox-3?

  • Acceleration / Vibrations / Stiffness resistance based on specific standart
  • Min Max for temperature and humidity
  • Power consumption
  • electromagnetic compatibility (EMC)
  • is it rugged
0 Kudos
Reply
1 Solution
380 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

We understand that this information is not provided. We do apologize.

The information that may be available is on regards of temperature, which is the following (only for RDB2):

"RDB2 is designed for room temperature environment.

The board may work abnormally or be damaged in the high/low temperature test."

And about rugged (we think so?):

DanielAguirre_0-1707922050902.png

Still, help us contacting your local NXP representative/FAE/DFAE, since they may more information available than the one we have through this channel. We do apologize.

Please, let us know.

View solution in original post

0 Kudos
Reply
1 Reply
381 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

We understand that this information is not provided. We do apologize.

The information that may be available is on regards of temperature, which is the following (only for RDB2):

"RDB2 is designed for room temperature environment.

The board may work abnormally or be damaged in the high/low temperature test."

And about rugged (we think so?):

DanielAguirre_0-1707922050902.png

Still, help us contacting your local NXP representative/FAE/DFAE, since they may more information available than the one we have through this channel. We do apologize.

Please, let us know.

0 Kudos
Reply