Getting to work Safety Peripheral Drivers example

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Getting to work Safety Peripheral Drivers example

1,217 Views
halilmutlu
Contributor II

I have installed SPD 1.01 as part of the Automative Software Package Manager bundle. But I could not get SPD example to work, configuration tools throws an error as:

Issue: Processor '' detected in NXP GCC 9.2 for Arm 32-bit Bare-Metal project does not match with currently selected `S32G274A_Rev2`. Target processor not supported or the computer is not on-line.
Level: Error
Type: Tool problem
Tool: McuConfiguration
Origin: SPD_101_S32G274_Rev2_M7_0
Resource: Processor
Information: -

Furthermore, the main.c in the example is empty (only the template main is there). Is there anyone having the same issue?

 

0 Kudos
Reply
0 Replies