Getting started with Yocto for NXP Goldbox

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Getting started with Yocto for NXP Goldbox

1,054件の閲覧回数
_arpit_
Contributor I

I am new to NXP Goldbox and I want to run my code (which is already running on a Linux based system) into NXP Goldbox, so as i understand I will have to install the required packages in yocto environment. So, I have a few questions: 

 

1. If i am able to login into the yocto env in root, will it directly get connected to internet if I connect the board to ethernet cable (via router)

2. Can i directly install any libraries in the goldbox through the shell access or is it necessary to install the libraries in yocto.

 

Requesting you to kindly support regarding the same .

0 件の賞賛
返信
1 返信

1,040件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @_arpit_ 

Thanks for your post.

I noticed that you have raised similar question, I will direct reply you via that thread.

Sorry for your inconvenience.

 

BR

Chenyin

0 件の賞賛
返信