FreeRtos image build for s32G

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FreeRtos image build for s32G

1,311 Views
ganireddy_vikash
Contributor I

Hi,

I want to build a FreeRTOS image for the NXP S32G processor and flash it to the target. However, I couldn’t find the steps required to generate the image. I have installed S32 Design Studio, but I’m unsure if I can use it for this purpose. If it is possible, please provide the necessary steps. Additionally, I couldn’t find any FreeRTOS-related plugins (*.zip) in S32 Studio or under software products. Please guide me on how to proceed.

followed:https://community.nxp.com/t5/S32G/S32G399A-RDB3-Guide-to-configure-FreeRTOS/m-p/1968846
but I didnt find any software:Automotive SW - S32G - FreeRTOS (Cortex-M7)  freertos

0 Kudos
Reply
4 Replies

1,299 Views
Joey_z
NXP Employee
NXP Employee

hi,ganireddy_vikash

Thank you for contacting us.

You can get information through this link:Design : Product Information : Automotive SW – S32G Reference Software ,  you also can find the S32G - FreeRTOS (Cortex-M7) as the following picture. 

Hope it can help you.

BR

Joey

0 Kudos
Reply

1,264 Views
ganireddy_vikash
Contributor I

Hi, Iam Unable find or download the package getting the following NOTE "Our records indicate that you have previously requested an Evaluation version for this product. If you would like to purchase the full product please visit us at NXP or contact your sales representative."

Thanks & Regards,
Vikash

 

 

0 Kudos
Reply

1,257 Views
Joey_z
NXP Employee
NXP Employee

hi,ganireddy_vikash

Thank you for your reply.

You will need to contact your FAE or sales representative to get permission for you.

BR

Joey

0 Kudos
Reply

1,263 Views
ganireddy_vikash
Contributor I
 
0 Kudos
Reply