Flexray could not transmit pdu

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flexray could not transmit pdu

772件の閲覧回数
zyt
Contributor III

I use two flexray node to connect together, they can both transfer to POC active.

but when I try to transmit pdu from one node, the flag bit MBIF can never be set and status always return busy. The other node can also not get MBIF set.

What might be the proble is?

0 件の賞賛
返信
1 返信

742件の閲覧回数
Joey_z
NXP Employee
NXP Employee

hi,zyt

In order to provide you with better help, please provide more information.
Which version of the LLCE driver are you using? Does your question use any routines?
Do you use custom boards? If not, is it an RDB or EVB board?

BR

Joey

0 件の賞賛
返信