ECC key pair format

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

ECC key pair format

跳至解决方案
2,580 次查看
Jeff-CF-Huang
Contributor III

Hi Sir,

I can generate a ECC key pair like this.

-----BEGIN PRIVATE KEY-----
MIGHAgEAMBMGByqGSM49AgEGCCqGSM49AwEHBG0wawIBAQQgEKbBHDa1DSl01d9c
kRoXkD866VoGC+Zi8j3CsFEJB06hRANCAASAaYdAi8oA7XJR5OHjpc7DTCoQ3JYU
sCPK8LhzyHVZDVCn7YTddZztpaFD92e0TLUjLEE2shv9LXlPN1N81+Sw
-----END PRIVATE KEY-----

-----BEGIN PUBLIC KEY-----
MFkwEwYHKoZIzj0CAQYIKoZIzj0DAQcDQgAEgGmHQIvKAO1yUeTh46XOw0wqENyW
FLAjyvC4c8h1WQ1Qp+2E3XWc7aWhQ/dntEy1IyxBNrIb/S15TzdTfNfksA==
-----END PUBLIC KEY-----

But, I don't know  how to convert them like below example.
Is there any way/tool to do it?

/* ECC NIST-P256 Key Pair */
static uint8_t eccP256BootKeyPub[] =
{
/*Qx*/
0xd6, 0x60, 0x62, 0x71, 0x13, 0x1e, 0x7e, 0x7e, 0x61, 0x7a, 0x81, 0xaa, 0x11, 0xf0, 0x9e, 0x7e,
0xd5, 0x63, 0x11, 0x82, 0x88, 0x23, 0x36, 0x7a, 0x86, 0x9b, 0x45, 0x40, 0x40, 0xb3, 0xf9, 0x05,
/*Qy*/
0xcf, 0x48, 0x97, 0x76, 0x61, 0x31, 0xaa, 0x8b, 0x7f, 0x80, 0x45, 0x3a, 0x15, 0xbf, 0x90, 0xf7,
0x51, 0x78, 0x78, 0x57, 0x9d, 0x5a, 0x4f, 0x97, 0x3a, 0xea, 0x5b, 0xb1, 0x15, 0x42, 0xe0, 0x7f
};
static uint8_t eccP256BootKeyPriv[] =
{
/*k*/
0x00, 0xd0, 0x07, 0xe1, 0xb9, 0xaf, 0xcc, 0x31, 0x2e, 0xec, 0x9c, 0xec, 0xff, 0xa0, 0x28, 0x07,
0x52, 0xbb, 0xd1, 0x95, 0x31, 0x82, 0xed, 0xef, 0x12, 0xf3, 0xfc, 0x36, 0x6e, 0x8f, 0x43, 0x56
};

0 项奖励
回复
1 解答
2,455 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Thanks for the feedback. For what we can see under the S32G tools, there is no Qx/Qy generation. It seems that you should be able to use OpenSSL for this situation, but we don't see any documentation on this specific regard (inside the S32G related documentation). We do apologize.

Please, let us know.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,536 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @Jeff-CF-Huang 

Which device are you using?

0 项奖励
回复
2,524 次查看
Jeff-CF-Huang
Contributor III
S32G234M & S32G399
0 项奖励
回复
2,456 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Thanks for the feedback. For what we can see under the S32G tools, there is no Qx/Qy generation. It seems that you should be able to use OpenSSL for this situation, but we don't see any documentation on this specific regard (inside the S32G related documentation). We do apologize.

Please, let us know.

0 项奖励
回复