EB tree 29.0.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,260件の閲覧回数
liujian_abup
Contributor I

hi,NXP:
   I was able to build it using a full project, but when I executed the launch.bat file, I couldn't find the corresponding make compiler. Moreover, the compiler in S32 doesn't have a make.exe compiler either. So, I need to use the 32-bit mingw compiler for Windows

0 件の賞賛
返信
1 解決策
1,238件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @liujian_abup 

Thanks for the post.

For building the project configured by EB, we suggest referencing the 5.3 part of AN13750(https://www.nxp.com/webapp/Download?colCode=AN13750), Cygwin is used and the compiler for the building is set with the GCC installation path from S32DS.

 

BR

Chenyin

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,239件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @liujian_abup 

Thanks for the post.

For building the project configured by EB, we suggest referencing the 5.3 part of AN13750(https://www.nxp.com/webapp/Download?colCode=AN13750), Cygwin is used and the compiler for the building is set with the GCC installation path from S32DS.

 

BR

Chenyin

0 件の賞賛
返信
%3CLINGO-SUB%20id%3D%22lingo-sub-2082500%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3EEB%20%E3%83%84%E3%83%AA%E3%83%BC%2029.0.0%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-2082500%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CP%3E%E3%81%93%E3%82%93%E3%81%AB%E3%81%A1%E3%81%AF%E3%80%81NXP%EF%BC%9A%3CBR%20%2F%3E%E3%83%95%E3%83%AB%E3%83%97%E3%83%AD%E3%82%B8%E3%82%A7%E3%82%AF%E3%83%88%E3%82%92%E4%BD%BF%E3%81%A3%E3%81%A6%E3%83%93%E3%83%AB%E3%83%89%E3%81%A7%E3%81%8D%E3%81%BE%E3%81%97%E3%81%9F%E3%81%8C%E3%80%81launch.bat%20%E3%83%95%E3%82%A1%E3%82%A4%E3%83%AB%E3%82%92%E5%AE%9F%E8%A1%8C%E3%81%97%E3%81%9F%E3%81%A8%E3%81%93%E3%82%8D%E3%80%81%E5%AF%BE%E5%BF%9C%E3%81%99%E3%82%8B%20make%20%E3%82%B3%E3%83%B3%E3%83%91%E3%82%A4%E3%83%A9%E3%81%8C%E8%A6%8B%E3%81%A4%E3%81%8B%E3%82%8A%E3%81%BE%E3%81%9B%E3%82%93%E3%81%A7%E3%81%97%E3%81%9F%E3%80%82%E3%81%95%E3%82%89%E3%81%AB%E3%80%81S32%E3%81%AE%E3%82%B3%E3%83%B3%E3%83%91%E3%82%A4%E3%83%A9%E3%81%AB%E3%81%AF%20make.exe%20%E3%82%B3%E3%83%B3%E3%83%91%E3%82%A4%E3%83%A9%E3%82%82%E3%81%82%E3%82%8A%E3%81%BE%E3%81%9B%E3%82%93%E3%80%82%E3%81%A0%E3%81%8B%E3%82%89%E3%80%81Windows%E7%94%A8%E3%81%AE32%E3%83%93%E3%83%83%E3%83%88mingw%E3%82%B3%E3%83%B3%E3%83%91%E3%82%A4%E3%83%A9%E3%82%92%E4%BD%BF%E7%94%A8%E3%81%99%E3%82%8B%E5%BF%85%E8%A6%81%E3%81%8C%E3%81%82%E3%82%8A%E3%81%BE%E3%81%99%3C%2FP%3E%3C%2FLINGO-BODY%3E