EB tree 29.0.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

EB tree 29.0.0

Jump to solution
1,272 Views
liujian_abup
Contributor I

hi,NXP:
   I was able to build it using a full project, but when I executed the launch.bat file, I couldn't find the corresponding make compiler. Moreover, the compiler in S32 doesn't have a make.exe compiler either. So, I need to use the 32-bit mingw compiler for Windows

0 Kudos
Reply
1 Solution
1,250 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @liujian_abup 

Thanks for the post.

For building the project configured by EB, we suggest referencing the 5.3 part of AN13750(https://www.nxp.com/webapp/Download?colCode=AN13750), Cygwin is used and the compiler for the building is set with the GCC installation path from S32DS.

 

BR

Chenyin

View solution in original post

0 Kudos
Reply
1 Reply
1,251 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @liujian_abup 

Thanks for the post.

For building the project configured by EB, we suggest referencing the 5.3 part of AN13750(https://www.nxp.com/webapp/Download?colCode=AN13750), Cygwin is used and the compiler for the building is set with the GCC installation path from S32DS.

 

BR

Chenyin

0 Kudos
Reply