Debugging Linux application on S32G-VNP-RDB2 using S32G Debug Probe

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Debugging Linux application on S32G-VNP-RDB2 using S32G Debug Probe

1,409 次查看
prafull_barpute
Contributor I

I am designing Linux based application using S32G-VNP-RDB2.

I received board and Linux SD card. I can able to boot board and able access board over UART0 using minicom.

I have also purchased S32G Debug probe. Now I want to connect this probe to board and start my development using S32G Design Studio. I want to using only single A53 core in my application.

When I tried open debugger configuration, no any device is present (please find attached screenshot for more detail) 

prafullb_0-1647953127005.png

Is it possible to use S32G Design Studio and S32Debugger port to configure peripherals and develop Linux based application.? Can anybody please guide me how to proceed now. 

Additional Information :

Debugger drivers are installed properly and Tx/Rx LED is blinking as well as RUN/PAUSE LED is constantly glowing as RED.

标记 (2)
0 项奖励
回复
0 回复数