DMA based UART using LINFlexd

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

DMA based UART using LINFlexd

跳至解决方案
4,359 次查看
noorhasan
Contributor III

Hello,

 

We are trying to use LINFlexd for UART communication in DMA based implementation.

While the same Linflexd channel can be used successfully when we use it with interrupt based implementation, I can't see data being transferred after the DMA0_Ch0 ISR is triggered for DMA based implementation.

Some of the inconsistencies that we observed is related to LIN register values when Tx is triggered.

When we select UART mode in UARTCR, as per the reference manual LINTCSR[mode] should always be set to 1 (UART mode). But, as shown in the screenshot below, it is still set in LIN mode, while UARTCR is in UART Mode.

 

noorhasan_1-1711568966912.png

 

 

noorhasan_0-1711568945889.png

 

noorhasan_2-1711568986109.png

 

noorhasan_3-1711569027395.png

 

noorhasan_4-1711569032492.png

 

 

Further, the data registers are both showing not-accessible (????)

 

noorhasan_5-1711569083583.png

 

 

Although, before the actual data transfer, the data registers are accessible:

noorhasan_6-1711569124056.png

 

Thank you for helping.

 

@justinlydick @haoyue-yan 

 

 

0 项奖励
回复
1 解答
4,346 次查看
haoyue-yan
NXP Employee
NXP Employee

Please close this ticket, the issue is being tracked else where.

 

Thanks

在原帖中查看解决方案

0 项奖励
回复
5 回复数
3,059 次查看
ssimpson
Contributor II

Hello, I would also be interested in knowing the answer to this question.
The above link notes that I do not have adequate permissions to view the answer.

0 项奖励
回复
3,640 次查看
Yhh1993
Contributor I
Hello, how did you solve it afterwards
0 项奖励
回复
4,347 次查看
haoyue-yan
NXP Employee
NXP Employee

Please close this ticket, the issue is being tracked else where.

 

Thanks

0 项奖励
回复
3,643 次查看
Yhh1993
Contributor I
I also encountered the same problem. Where is the solution document,thanks!
0 项奖励
回复
4,349 次查看
noorhasan
Contributor III

Please close this post as it is now being followed through a new post:

 

https://community.nxp.com/t5/GM-MCU3-PMIC3-Product-Support/Question-from-GM-DMA-based-UART-using-LIN...

 

0 项奖励
回复