Hi all,
I have been working with the S32G399A-RDB3 board and have built a custom Yocto image based on your provided BSP, with some modifications.
I've purchased the S32G-VNP-GLDBOX3 board and would like to confirm the following:
Can I use the same Yocto BSP and image that I built for the S32G399A-RDB3 directly on the GoldBox 3?
Are there any differences in device trees, hardware configurations (e.g., Ethernet PHYs, PMICs, USB transceivers), or bootloader settings that I should be aware of?
Do you provide a separate BSP or machine configuration specific to GoldBox 3?
I would appreciate your guidance to ensure a smooth transition without compatibility issues.