CAN Gateway Slow Path

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CAN Gateway Slow Path

1,426件の閲覧回数
akhil_k_appu
Contributor III

For running the Cortex-M7 slow-path use cases, we set the  SW12 in ON-ON position. After this we need to run the  A53 slow-path use cases.

Is it required to make SW12 in ON-OFF Position ??

0 件の賞賛
返信
2 返答(返信)

1,415件の閲覧回数
gmocanu
NXP Employee
NXP Employee

Hello,

 

You can keep SW12 in ON-ON position. This configuration is needed only to load a custom FW and switch table on SJA that are required for the cloud connectivity use case, and the M7-core-based routing. The other use cases / demos are not affected by this configuration.

 

Best regards,

George

0 件の賞賛
返信

1,408件の閲覧回数
akhil_k_appu
Contributor III

Thank you @gmocanu 

0 件の賞賛
返信