CAN Gateway Slow Path

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CAN Gateway Slow Path

1,432 次查看
akhil_k_appu
Contributor III

For running the Cortex-M7 slow-path use cases, we set the  SW12 in ON-ON position. After this we need to run the  A53 slow-path use cases.

Is it required to make SW12 in ON-OFF Position ??

0 项奖励
回复
2 回复数

1,421 次查看
gmocanu
NXP Employee
NXP Employee

Hello,

 

You can keep SW12 in ON-ON position. This configuration is needed only to load a custom FW and switch table on SJA that are required for the cloud connectivity use case, and the M7-core-based routing. The other use cases / demos are not affected by this configuration.

 

Best regards,

George

0 项奖励
回复

1,414 次查看
akhil_k_appu
Contributor III

Thank you @gmocanu 

0 项奖励
回复