CAN / CAN-FD to ETH Routing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAN / CAN-FD to ETH Routing

1,829 Views
gautamvarun23
Contributor I

How can I configure CAN / CAN-FD to ETH Routing

please provide me some information

0 Kudos
Reply
3 Replies

1,814 Views
shanlan123
Contributor II
do you solved the problem?
问题解决了吗
0 Kudos
Reply

1,819 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

We could recommend first looking into the "AN13423 - Using CAN2CAN, CAN2ETH and ETH2CAN Features of LLCE on S32G", which is available on the S32G2 product page (link: S32G2 Safe and Secure Vehicle Network Processor | NXP Semiconductors)

There is an example application for this situation provided on the "LLCE Driver + Firmware" for S32G platform. This should be found (once LLCE Driver + Firmware is installed) on the following address:

"C:\nxp\S32G_LLCE_1_0_4\sample_app_llce\llce_sample_app_pfe"

Also, more information is provided on the LLCE Firmware User Guide on chapter 1.3.5 Ethernet Communication [v1.0.4]. This should be available (once LLCE Driver + Firmware is installed) on the following address:

"C:/nxp/S32G_LLCE_1_0_4/firmware/llce_interface/doc/LLCE_firmware_user_guide.pdf"

Please, let us know if this information was helpful or not.

0 Kudos
Reply

1,809 Views
shanlan123
Contributor II
C:\nxp\S32G_LLCE_1_0_4\sample_app_llce\llce_sample_app_pfe.the config of EB Tresos seems wrong.
0 Kudos
Reply