BSP31 points to invalid pfeng driver repo commit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BSP31 points to invalid pfeng driver repo commit

Jump to solution
2,712 Views
f_frank
Contributor I

After upgrading from BSP30 to recently released BSP31 for S32G, the pfe recipe points to a not (yet) committed revision in pfeng repository. Same unreleased revision is also referenced by libfci_0.9.6.bb.

Am I missing some step here or is the driver not yet released to that repo. What is the timeline to commit it?

@jpetrous tagging you since most commits in pfeng repo were done by you.

Tags (3)
0 Kudos
Reply
1 Solution
2,705 Views
bpe
NXP Employee
NXP Employee

Automotive BSP 31 has not been officially released. Early code drops currently available
through GIT repositories may have certain issues. Full support in the Community
will be available when the official BSP 31 release is made. Until then, our
main recommendation is, stay with BSP 30.0. A limited support to BSP 31 code
drops can be requested via tickets, our answers depend on availability of the SW development
team members for internal discussion.

Best Regards,
Platon

 

View solution in original post

2 Replies
2,560 Views
lakehu
Contributor II

When bsp31 could have a official open release with PFE ??

Thanks 

0 Kudos
Reply
2,706 Views
bpe
NXP Employee
NXP Employee

Automotive BSP 31 has not been officially released. Early code drops currently available
through GIT repositories may have certain issues. Full support in the Community
will be available when the official BSP 31 release is made. Until then, our
main recommendation is, stay with BSP 30.0. A limited support to BSP 31 code
drops can be requested via tickets, our answers depend on availability of the SW development
team members for internal discussion.

Best Regards,
Platon