Adding git package in linux image for S32G2

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Adding git package in linux image for S32G2

738 次查看
Vishnu3
Contributor III

Hi all,

 

I am trying to build the linux image for S32G2 as per the document "Linux BSP 33.0 User Manual for S32G2 platforms" provided by NXP.

 

I am able to build the basic image "fsl-image-auto" and boots well on my S32G2 device. 

 

Now I would like to use git commands on my S32G2 terminal. 

 

How do I bitbake git package into my linux image? 

I have tried to add the git by making the following changes in the local.conf file in the build folder


IMAGE_INSTALL_append = " git"

 

and then bitbaking the image. But the git command is still not installed in the image. Please give some pointers. I am fairly new to Yocto. 

 

Best,

 

Vishnu

标记 (3)
0 项奖励
回复
1 回复

716 次查看
chenyin_h
NXP Employee
NXP Employee

Hello, @Vishnu3 

Thanks for your post.

Yes, git package is not by default included in the BSP release, I feel sorry for your inconvenience.

This is Yocto related, you may reference the formal documents from Yocto to try adding addtional packages .

From my experience,  the following way may take effect and is only for your reference, you may firstly copy the git directory from Yocto to the meta-alb/recipes-devtools directory, also add IMAGE_INSTALL_append = " git" to your conf/local.conf, and then use the bitbake fsl-image-auto to have a try.

 

BR

Chenyin

0 项奖励
回复