Access to eIQ auto ML toolkit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Access to eIQ auto ML toolkit

1,169件の閲覧回数
Geonha_
Contributor I

Hello!

I'm planning to use the GOLDBOX3 platform from NXP to research model optimization methods for machine learning applications in a vehicle-embedded environment.

To achieve this, I aim to explore performance baselines and investigate optimization methods using the NXP-AUTO-ML toolkit.

My question is, without signing an NDA, is it completely inaccessible?

In the presentation here(https://www.nxp.com/design/design-center/training/TIP-ACCELERATING-VEHICLE-INTELLIGENCE-MACHINE-LEAR), it mentions that a standard version is also available, but I haven’t been able to locate it anywhere.

If anyone has had similar concerns, I’d appreciate any advice.

Thank you!!

ラベル(1)
0 件の賞賛
返信
1 返信

1,143件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @Geonha_ 
Thanks for your post.

As far as I know, when sharing with the AI related packages to the customer, they have all signed the NDAs.

I could help to double confirm it, if there is any changes(if the standard version could be used without NDA), I will update the status here.

 

BR

Chenyin

0 件の賞賛
返信