Dear NXP fellows,
This questions is related to my previous question.
I would like to get a better understanding of the pin mux and how does it relate the hardware pin to the device tree mapping.
Let's suppose I am using S32G274ARDB board with BSP35.0.
When I look at the schematic design file of the board I see that it uses the PFE_MAC2 to connect to the Micrel KSZ9031 Phy Device through RGMII:

So, if I look at the schematic of the KSZ9031 device, I see that its pin 25 (TX_EN) is connected to the signal RGMIIB_TXC, which corresponds to the pin V20 (PFE_MAC2_TX_CLK) of the P32G274AABK1VUCT:

Ok, so if I take a look at the Kernel device tree file s32gxxxx.dtsi, I see that the pfe_netif2 (PFE_MAC2) is using phy-handle = <&pfe_mdio_b_phy4> or ethernet-phy@4 and pfe2rgmiib_pins is defined in the following way:
pfe2rgmiib_pins: pfe2rgmiib_pins {
pfe2rgmiib_grp0 {
pinmux = <S32CC_PINMUX(78, FUNC2)>,
<S32CC_PINMUX(144, FUNC2)>,
<S32CC_PINMUX(113, FUNC2)>,
<S32CC_PINMUX(114, FUNC2)>,
<S32CC_PINMUX(115, FUNC2)>;
output-enable;
slew-rate = <S32CC_FAST_SLEW_166MHZ>;
};
pfe2rgmiib_grp1 {
pinmux = <S32CC_PINMUX(116, FUNC0)>,
<S32CC_PINMUX(117, FUNC0)>,
<S32CC_PINMUX(118, FUNC0)>,
<S32CC_PINMUX(119, FUNC0)>,
<S32CC_PINMUX(120, FUNC0)>,
<S32CC_PINMUX(121, FUNC0)>;
input-enable;
slew-rate = <S32CC_FAST_SLEW_166MHZ>;
};
pfe2rgmiib_grp2 {
pinmux = <S32CC_PINMUX(879, FUNC3)>,
<S32CC_PINMUX(885, FUNC3)>,
<S32CC_PINMUX(881, FUNC3)>,
<S32CC_PINMUX(882, FUNC3)>,
<S32CC_PINMUX(883, FUNC3)>,
<S32CC_PINMUX(884, FUNC3)>,
<S32CC_PINMUX(886, FUNC3)>;
};
pfe2rgmiib_grp3 {
pinmux = <S32CC_PINMUX(122, FUNC2)>;
output-enable;
slew-rate = <S32CC_FAST_SLEW_166MHZ>;
bias-pull-up;
};
};
Ok, from the file s32cc-pinfunc.h I see that the S32CC_PINMUX function is defined as follows:
#define FUNC0 0
#define FUNC1 1
#define FUNC2 2
#define FUNC3 3
#define FUNC4 4
#define FUNC5 5
#define FUNC6 6
#define FUNC7 7
#define S32CC_PINMUX(PIN, FUNC) (((PIN) << 4) | (FUNC))
Ok, so from an external repository, I found that definition:
#define S32_G274_PAD_PH10__PFE2_TXCLK_IN 886 PAD_CTL_SRC_SIG_SEL3
That means the PIN 886 corresponds to PH10__PFE2_TXCLK_IN.
And my questions are:
- Where does this number 886 comes from? Is there a documentation somewhere that associates this number with a specific pin in the hardware?
- What is the meaning of FUNC0, FUNC1, FUNC2, etc.?
- If in my custom board design I decide to replace Micrel KSZ9031 Phy Device by a Marvell Phy Device, can I still use the same pfe2rgmiib_pins or I need to adapt it to the current hardware?
Thank you very much for your support,
Best regards,
Guilherme