About CPU clock and CAN supply clock

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About CPU clock and CAN supply clock

ソリューションへジャンプ
2,406件の閲覧回数
kazuki
Contributor II

Please tell me about the sample project "Can_Llce_DS_Can2Can_S32G399A_M7".

I am investigating the CAN clock and CPU clock using S32DS.

Looking at the config of Can_43_LLCE
I found that CanCpuClokRef in the CanController settings refers to the MCU settings.
setting name="CanCpuClockRef" value="/Mcu_1/Mcu/McuModuleConfiguration/VS_0/CAN_PE_CLK"

CAN_PE_CLK was set to 4000000.
Are you aware that the CAN clock is 4000000Hz?
Also, I couldn't find any settings for the CPU clock.
Could you please tell me the CPU clock settings for the sample project?

0 件の賞賛
返信
1 解決策
2,207件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Thanks for your feedback. We might be misunderstanding the request, if so, we apologize.

We understand that you are saying that CAN_PE_CLK frequency is 40MHz, is this correct?

DanielAguirre_0-1711114193046.png

If so, it is correct. We understand that under the NXP examples, this is the frequency given to CAN_PE_CLK.

As for the CPU Frequency, should be XBAR_CLK the one that provides the CPU frequency:

DanielAguirre_1-1711114337576.png

Please, let us know.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,374件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Can you let us know with which LLCE/RTD package version are you working with?

Please, let us know.

0 件の賞賛
返信
2,364件の閲覧回数
kazuki
Contributor II

hello

thank you for your reply.

excuse me. It did not include version information.

The sample project used is the one included in S32G_LLCE_GATEWAY_1.0.5_QLP1_D2302.

The version is below.
LLCE:1.0.5
RTD: Real Time Drivers Version 4.0.0

This is the same version as LLCE and RTD described in 5. Configuring on S32CT of AN13423 in the document.

thank you.

0 件の賞賛
返信
2,208件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Thanks for your feedback. We might be misunderstanding the request, if so, we apologize.

We understand that you are saying that CAN_PE_CLK frequency is 40MHz, is this correct?

DanielAguirre_0-1711114193046.png

If so, it is correct. We understand that under the NXP examples, this is the frequency given to CAN_PE_CLK.

As for the CPU Frequency, should be XBAR_CLK the one that provides the CPU frequency:

DanielAguirre_1-1711114337576.png

Please, let us know.

0 件の賞賛
返信