Build NXP Auto Linux Yocto BSP on Windows using WSL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Build NXP Auto Linux Yocto BSP on Windows using WSL

Build NXP Auto Linux Yocto BSP on Windows using WSL

This document provides a step-by-step guide to building the NXP Auto Linux Yocto BSP using WSL 2 (Windows Subsystem for Linux) instead of a full virtual machine or native Linux installation. This approach is especially useful for developers working in Windows environments who want a faster and more streamlined way to set up their development environment for platforms like the S32G-VNP-RDB3.

The guide covers everything from installing WSL 2 and configuring system resources, to downloading the BSP, building it with Yocto, and flashing the image to an SD card. It also includes practical tips to help avoid common build issues.

 

ラベル(1)
添付
評価なし
バージョン履歴
最終更新日:
‎05-28-2025 01:27 PM
更新者: