the difference between library with FP (softfp) and library with FP (hard) in s32k144

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

the difference between library with FP (softfp) and library with FP (hard) in s32k144

935 Views
zhangchun
Contributor III

hello

I tested library with FP (softfp) and FP instructions(hard) using the attached example.

zhangchun_0-1691412399611.jpeg

 

 

I found that there is no difference in performance between these two floating-point operations. However, from this document(S32K14x系列MCU使用Tips之硬件FPU特性介绍和使用详解 ), it can be seen that hard uses fpu registers, which should have a more significant improvement in floating-point performance.

zhangchun_1-1691412399645.png

 

 

Now, I don't quite understand how to use hardware floating-point operations in S32K44

thanks

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

780 Views
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @zhangchun , 

Closing this case as it was answered in the other post: 

 

https://community.nxp.com/t5/S32-Design-Studio/the-difference-between-library-with-FP-softfp-and-lib...

 

Thank you. Best regards. 

- Mehul Patel 

 

0 Kudos
Reply