s32k144 lin sdk example

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

s32k144 lin sdk example

跳至解决方案
5,348 次查看
sohyunjang
Contributor III

Hi, I use lin slave sdk example in S32 Design Studio for ARM v1.3

I was having trouble reading the Lin_slave.dox document in the Doxtgen folder.

I use S32K144EVB-Q100. But, What does S32K144-MB mean?

And

   PIN FUNCTION    |   S32K144EVB-Q100         |   S32K144-MB
    ----------------|---------------|--------------
    BUTTON 2 (\b PTC13) |BTN1  - wired on the board  |   BTN3 - wired on the board
    BUTTON 1 (\b PTC12) |BTN0  - wired on the board  |   BTN2 - wired on the board
    RED_LED (\b PTD15) |RGB_RED - wired on the board    |   J12.17 - J11.31
    GREEN_LED (\b PTD16) |RGB_GREEN - wired on the board  | J12.16 - J11.30
    BLUE_LED (\b PTD16) |RGB_GREEN - wired on the board  |  J12.31 - J11.29
    GND       (\b GND)  |J3-11 - Master GND    |J6 - Master GND
    LPUART2_RX (\b PTD6) |J5-18 - J4-6 | J12.25 - J10.17
    FTM0_CH5 (\b PTB17) |J4.6 - J5.18 | J10.17 - J12.25
    LIN (\b *)             |J11-1 - Master LIN |  J48.4 - Master LIN

    <b>(*) Those lines must be modulated using a transceiver, if it is not specified the boards already include the LIN transceiver</b>

  GND       (\b GND)  |J3-11 - Master GND    |J6 - Master GND
    LPUART2_RX (\b PTD6) |J5-18 - J4-6 | J12.25 - J10.17
    FTM0_CH5 (\b PTB17) |J4.6 - J5.18 | J10.17 - J12.25
    LIN (\b *)             |J11-1 - Master LIN |  J48.4 - Master LIN

What does it mean?

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
4,686 次查看
raresvasile
NXP Employee
NXP Employee

Hi,

Yes, you have to connect them using a cable from J5-18 - J4-6(on the board headers).

Best regards,

Rares

在原帖中查看解决方案

0 项奖励
回复
3 回复数
4,686 次查看
raresvasile
NXP Employee
NXP Employee

Hi, 

The S32K144-MB is an internal board, used for validation.

Best regards,

Rares

0 项奖励
回复
4,686 次查看
sohyunjang
Contributor III

Hi,

Do I need to connect the two wires?

    LPUART2_RX (\b PTD6) |J5-18 - J4-6 | J12.25 - J10.17
    FTM0_CH5 (\b PTB17) |J4.6 - J5.18 | J10.17 - J12.25

Thank you.

0 项奖励
回复
4,687 次查看
raresvasile
NXP Employee
NXP Employee

Hi,

Yes, you have to connect them using a cable from J5-18 - J4-6(on the board headers).

Best regards,

Rares

0 项奖励
回复